When a fault occurs, the drive fault relay is opened, the output stage is switched off (motor loses all torqueTorque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist), or the load is dynamically braked. The specific drive behavior depends on the type of fault. The LED display on the front panel of the drive shows the number of the fault that occurred. If a warning is issued prior to the fault, the warning is shown on the LED and has the same number as the associated fault. Warnings do not trip the power stage of the drive or fault relay output.
The left side of the LED displays F for a fault or n for a warning. The right side displays the fault or warning number as follows: 1-0-1-[break]. The highest priority fault is displayed on the LED. Multiple faults may be present when a fault condition is occurring. Check theWorkBench Fault Screen or read the status of DRV.FAULTS through the controller or HMI"Human-machine interfaces " Also known as computer-human interfaces (CHI), and formerly known as man-machine interfaces, they are usually employed to communicate with PLCs and other computers, such as entering and monitoring temperatures or pressures for further automated control or emergency response for the entire list of faults.
Clearing Faults
Most faults can be cleared without cycling power to the drive (unless they are specifically noted in the table as requiring 24 V power cycle).
|
Fault |
Message/Warning |
Cause |
Remedy |
DriveControl device for regulating the speed, torque and position of a motor Response to Fault |
|---|---|---|---|---|
|
|
Reserved. |
N/A |
N/A | |
|
|
Firmware incompatible. |
Installed firmware is not compatible with the drive hardware. |
Load compatible firmware into the drive. |
Disable power stage |
| The FPGA"Field-Programmable Gate Array" FPGA is a semiconductor device that can be configured by the customer or designer after manufacturing; hence the name "field-programmable" is a lab FPGA. | The FPGA is a lab version FPGA. | Load the released FPGA version that is compatible with the operational firmware. | None | |
|
Resident Firmware failed. |
Software failure detected. |
Restart drive. If issue persists, contact technical support. |
Disable power stage | |
| Operational FPGA is not a default FPGA. | The FPGA minor version is larger than the operational firmware default FPGA minor version | Load the released FPGA version that is compatible with the operational firmware. | None | |
|
Resident FPGA failed. |
Software failure detected. Load resident FPGA failure occurred (several cases according to flowchart, including incompatible image to FPGA type and fieldbus type). |
Restart drive. If issue persists, contact technical support. |
Disable power stage | |
|
Operational FPGA failed. |
Software failure detected. Load operational FPGA failure occurred (several cases according to flowchart). |
Restart drive. If issue persists, contact technical support. |
Disable power stage | |
|
NV Memory Stamp. |
Non-volatileinformation is stored in a specific memory to remain accessible even when the application has been powered off memory stamp is corrupted or invalid. |
ResetNew start of the microprocessor the drive to default memory values using Parameter Load in WorkBench. |
Disable power stage | |
|
NV Memory Data (might occur when downloading firmware). |
Non-volatile memory data is corrupted or invalid. When this fault occurs after a firmware download, it is not an indication of a problem (clear the fault and perform a “save” to the drive). |
Reset the drive to default memory values using Parameter Load in WorkBench. |
Disable power stage | |
|
n107 |
Positive switch. |
Positive position limit is exceeded. |
Move the load away from the limits. |
Controlled stop |
|
n108 |
Negative switch. |
Negative position limit is exceeded. |
Move the load away from the limits. |
Controlled stop |
|
Drive did not finish homing sequence. |
Check homing sensorA sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer, homing mode, and homing configuration. |
Controlled stop | ||
|
n123 |
Invalid motion task. |
Invalid motion task. |
Check motion task settings and parameters to make sure that the values entered will produce a valid motion task. |
Disable power stage |
|
n125 |
The fieldbus lost synchronization. |
Check fieldbus connection (X5 and X6 if you are using EtherCATEtherCAT is an open, high-performance Ethernet-based fieldbus system. The development goal of EtherCAT was to apply Ethernet to automation applications which require short data update times (also called cycle times) with low communication jitter (for synchronization purposes) and low hardware costs; X12 and X13 if you are using CANopen) or the settings of your EtherCAT or CANopen master. |
Controlled stop | |
|
n126 |
Bode plot too much movement. |
Too much movement was created during a Bode plot. Motor is unstable and is not following drive instructions. |
Check that the system is closed loop stable. Refer to the system tuning guide. |
Dynamic braking |
|
Incomplete Emergency Procedure. |
Incomplete emergency stop procedure (problem with the emergency stop motion task). |
Disconnect power from drive and check emergency stop procedure. |
Dynamic braking | |
|
Mpoles / Fpoles not integer. |
Ratio of motor poles to feedback poles must be a whole number. |
Disable power stage | ||
|
Fieldbus Heartbeat lost. |
Heartbeat lost. |
Check CANopen cabling. Reduce bus load or increase the heartbeat update time. |
Controlled stop | |
|
Secondary feedback supply over current. |
5V power supply was shorted out on X9. |
Check X9 connection. |
Disable power stage | |
|
Secondary feedback A/B line break. |
Problem in secondary feedback detected. |
Check secondary feedback (X9 connection). |
Disable power stage | |
|
Secondary feedback Z line break. |
Problem in secondary feedback detected. |
Check secondary feedback (X9 connection). |
Disable power stage | |
| Fault number changed to to F138. See F138 for details. | Disable power stage | |||
|
Secondary feedback illegal state. |
Feedback signals were detected in an illegal combination. |
Check X9 connection. |
Disable power stage | |
|
n135 |
Fault on FB2 is preventing remote commutation for FB1. |
Attempt to issue motion task before the axis is homed. Axis must be homed before motion task can start. |
Change opmode or home axis. |
Disable power stage |
|
Firmware and FPGA versions are not compatible. |
The FPGA version does not match the firmware FPGA version constants. | Load the FPGA version that is compatible with the firmware. | Disable power stage | |
| Homing and feedback mismatch | The configured homing mode is not supported by the motor feedback type used. | Change homing mode. | None | |
|
Instability during autotune. |
Drive current (IL"Instruction list" This is a low-level language and resembles assembly.CMD) or velocity feedback (VL.FB) exceeds allowable limit (BODE.IFLIMIT or BODE.VFLIMIT). This fault only occurs in BODE.MODE 5. This fault often occurs when complex mechanics, belts, and compliant loads are present. | Change BODE.MODE if appropriate. If BODE.MODE 5 is appropriate and the fault occurs at the end of an Autotuning, then the motor is not robustly stable. You can manually adjust Autotuner settings. Manual tuning may be required to make the motor stable. | Controlled stop | |
| F139 |
Target position was overshot due to invalid motion task activation. |
The drive cannot decelerate from its current speed to reach the end point of the second motion task without moving past it. Increase the deceleration rate in the move or trigger the move earlier. | Change Motion task profile and clear fault with DRV.CLRFAULTS. Or change the value of FAULT139.ACTION = 1 to ignore this condition. | Disable power stage |
| n140 | VBUS.HALFVOLT has changed. Save the parameters and reboot the drive. | The user has changed the numerical value of VBUS.HALFVOLT. This change only takes effect after a DRV.NVSAVE command and after rebooting the AKD. | Save the parameters in the non-volatile memory via a DRV.NVSAVE command and turn off/on the 24[V] power supply in order to reboot the drive or restore the original stetting of VBUS.HALFVOLT. | None |
| Not enough distance to move; motion exception. | For trapezoidal and customer table motion tasks:
The target velocity specified in the motion task cannot be reached via using the selected acceleration and deceleration since the distance to travel is not sufficient. For a 1:1 profile: The selected acceleration and deceleration will be extended since there is too much distance to travel and the motion task would exceed its maximum allowed velocity. |
Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. Check motion task settings and parameters to make sure that the values entered will produce a valid motion task. | None | |
| Not enough distance to move; following motion exception. | A new motion task activated, when one motion task is already active and the target position specified in the motion task parameters cannot be reached with specified target velocity, acceleration and deceleration parameters. The motion task will directly decelerate to into the target position or ramps down to velocity 0 and start another move to reach target position of the next motion task. | Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. Check motion task settings and parameters to make sure that the values entered will produce a valid motion task. | None | |
| Velocity limit violation, exceeding max limit. | A new target velocity calculated internally due to an exception, and is being limited due to user velocity limit. | Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. Check motion task target velocity settings and parameters to make sure that the values entered will not exceed the VL.LIMITP and VL.LIMITN setting. | None | |
| Following motion failed; check motion parameters. | Activation of the following motion task failed due to incompatible parameters, or motion task does not exist. | Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. Check following motion task settings and parameters to make sure that the values entered will produce a valid motion task. | None | |
| Target position crossed due to stop command. | The motion task crosses the target position after triggering a DRV.STOP command. This situation can happen when processing a change-on-the-fly motion task and triggering a DRV.STOP command close to the target position of the currently running motion task. | Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. | None | |
| Homing index pulse not found. | A homing mode with index detection is activated, and index pulse is not detected while moving across the range determined by the hardware limit switches. | Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. | None | |
| Homing reference switch not found. | A homing mode with reference switch detection is activated and the reference switch is not detected while moving across the range determined by the hardware limit switches. | Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. | None | |
| Failed to set motion task parameters | Invalid motion task parameters assignment. This warning can appear upon an MT.SET command. | Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. Check motion task settings and parameters. | None | |
| Motion task activation failed. | Activation of the motion task failed due to incompatible parameters, or motion task does not exist. This warning can appear upon an MT.MOVE command. | Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. Check motion task settings and parameters to make sure that the values entered will produce a valid motion task. | None | |
| Homing procedure failed. | Homing error observed during the operation of homing procedure. | Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. | None | |
| MT.NUM exceeds limit. | This warning appears with n160. This warning is triggered when you try to trigger a motion task > 128 (such as MT.MOVE 130). | Trigger only motion tasks between 0 and 128. Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. | None | |
| Motion task is not initialized. | This warning appears with n160. This warning is triggered when you try to trigger a non-initialized motion task. | Initialize the motion task first before starting the task. Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. | None | |
| Motion task target position is out. | This warning appears with n160. This warning is triggered when you try to trigger a motion task with an absolute target position outside of the selected modulo range (see also MT.CNTL). | Move the absolute target position of the motion task within the modulo range.Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. | None | |
| Invalid bit combination in the motion task control word. | This warning appears with n160. This warning is triggered when you try to trigger a motion task with an invalid bit combination in the motion task control word (see also MT.CNTL). | Correct the MT.CNTL setting for the specific motion task. Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. | None | |
| 1:1 profile cannot be triggered on the fly. | This warning appears with n160. This warning is triggered when you try to trigger a 1:1 profile table motion task while another motion task is currently running. | 1:1 profile table motion tasks should be started from velocity 0. Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. | None | |
| Customer profile table is not initialized. | This warning appears with n160. This warning is triggered when you try to trigger a motion task that uses a customer profile table for generating the velocity profile and when the selected profile table is empty (see MT.CNTL and MT.TNUM. | Change the MT.TNUM parameter for this specific motion task in order to use an initialized profile table. Activation of any new motion or using of DRV.CLRFAULTS will clear the warning. | None | |
|
Internal RAM failed. |
Hardware failure detected. |
Restart drive. If issue persists, contact technical support. |
Disable power stage | |
|
External RAM failed. |
Hardware failure detected. |
Restart drive. If issue persists, contact technical support. |
Disable power stage | |
|
Code Integrity failed. |
Software failure detected. FPGA register access failure occurred. |
Restart drive. If issue persists, contact technical support. |
Disable power stage | |
|
Control board EEPROM read failed. |
EEPROM failure detected. |
Restart drive. If issue persists, exchange drive. |
Disable power stage | |
|
Control board EEPROM corrupted serial num stamp. |
EEPROM failure detected. |
Restart drive. If issue persists, exchange drive. |
Disable power stage | |
|
Control board EEPROM corrupted serial num data. |
EEPROM failure detected. |
Restart drive. If issue persists, exchange drive. |
Disable power stage | |
|
Control board EEPROM corrupted parameter stamp. |
EEPROM failure detected. |
Restart drive. If issue persists, exchange drive. |
Disable power stage | |
|
Control board EEPROM corrupted parameter data. |
EEPROM failure detected. | Restart drive. If issue persists, exchange drive. | Disable power stage | |
|
Power board EEPROM read failed. |
EEPROM failure detected. | Restart drive. If issue persists, exchange drive. | Disable power stage | |
|
Power board EEPROM corrupted serial num stamp. |
EEPROM failure detected. | Restart drive. If issue persists, exchange drive. | Disable power stage | |
|
Power board EEPROM corrupted serial num data. |
EEPROM failure detected. | Restart drive. If issue persists, exchange drive. | Disable power stage | |
|
Power board EEPROM corrupted parameter stamp. |
EEPROM failure detected. | Restart drive. If issue persists, exchange drive. | Disable power stage | |
|
Power board EEPROM corrupted parameter data. |
EEPROM failure detected. | Restart drive. If issue persists, exchange drive. | Disable power stage | |
|
Control board EEPROM write failed. |
EEPROM failure detected. |
Restart drive. If issue persists, exchange drive. |
Disable power stage | |
|
Power board EEPROM write failed. |
EEPROM failure detected. |
Restart drive. If issue persists, exchange drive. |
Disable power stage | |
|
Power board EEPROM invalid data. |
EEPROM failure detected. |
Restart drive. If issue persists, exchange drive. |
Disable power stage | |
|
n234 |
Control over temperature sensor 1. |
High temperature limit reached. |
Check cabinet ventilation system. |
Disable power stage |
|
n235 |
Power over temperature sensor 1. |
|||
|
n236 |
Power over temperature sensor 2. |
|||
|
n237 |
Power over temperature sensor 3. |
|||
|
n240 |
Control under temperature sensor 1. |
Low temperature limit reached. |
Check cabinet ventilation system. |
Disable power stage |
|
n241 |
Power under temperature sensor 1. |
|||
|
n242 |
Power under temperature sensor 2. |
|||
|
n243 |
Power under temperature sensor 3. |
|||
|
External Fault. |
This fault is user generated and is caused by user settings. |
Users can configure a digital input to trigger this fault (DINx.MODE = 10). The fault occurs according to this input setting. Clear the input to clear the fault. |
Disable power stage | |
|
Vbus read is out of thresholds. |
Hardware problem in bus measurement. | Troubleshoot and repair hardware problem. | Disable power stage | |
| F248 |
Option board EEPROM corrupted. |
EEPROM failure detected. | Restart drive. If issue persists, exchange drive. | Disable power stage |
| F249 |
Option board downstream checksum. |
Communications with the I/O on the option board failed. | DRV.CLRFAULTS. If issue persists If issue persists, contact technical support. | Disable power stage |
| F250 |
Option board upstream checksum. |
Communications with the I/O on the option board failed. | DRV.CLRFAULTS. If issue persists If issue persists, contact technical support. | Disable power stage |
| F251 |
Option board watchdog. |
Communications with the I/O on the option board failed. | DRV.CLRFAULTS. If issue persists If issue persists, contact technical support. | Disable power stage |
| F252 |
Firmware and option board FPGA types are not compatible. |
The option board FPGA is not compatible with this hardware. | Download the correct firmware file for this drive. | Disable power stage |
| F253 |
Firmware and option board FPGA versions are not compatible. |
The version of the option board FPGA is not compatible with this firmware. | Download the correct firmware file for this drive. | Disable power stage |
|
F256 |
Analog Input over voltage | The analog input value is above the AIN.OVFTHRESH level. | Check the analog input signal or change the AIN.OVFTHRESH value. | Controlled Stop |
| F257 | Analog Input under voltage | The analog input value is below the AIN.UVFTHRESH level. | Check the analog input signal or change the AIN.UVFTHRESH value. | Controlled Stop |
| n256 | Warning: Analog Input over voltage | The analog input value is above the AIN.OVWTHRESH level. | Check the analog input signal or change the AIN.OVWTHRESH value. | None |
| n257 | Warning: Analog Input under voltage | The analog input value is below the AIN.UVWTHRESH level. | Check the analog input signal or change the AIN.UVWTHRESH value. | None |
|
n301 |
Motor overheated. |
Motor overheated. |
Check ambient temperature. Check motor mounting heat sink capability |
Disable power stage |
|
Over speed. |
Motor exceeded VL.THRESH value. |
Increase VL.THRESH or lower velocity command. |
Dynamic braking | |
|
Run away. |
Motor did not follow command values. |
Current command to the motor is too high for too long. Reduce servo gains, or reduce command trajectory aggressiveness. | Controlled stop | |
|
n304 |
Motor Foldback. |
Maximum motor power has been exceeded; the power has been limited to protect the motor |
Motion is requiring too much power. Change move profile to reduce load on motor. Check for load jamming or sticking. Check that current limits are set correctly. |
Controlled stop |
|
Brake open circuit. |
Motor brake open circuit. Fault threshold is 200 mA. |
Check cabling and general functionality. For special low current brake applications, the F305 fault can be bypassed using the setting motor.brake = 100. |
Dynamic braking | |
|
Brake short circuit. |
Motor brake short circuit. |
Check cabling and general functionality. Check that MOTOR.TBRAKERLS on pg. 1 and MOTOR.TBRAKEAPP on pg. 1 are configured. |
Dynamic braking | |
|
Brake applied during EnableEnable signal for the drive, Hardware-Enable with 24V signal to X8, Software-Enable command by setup Software, fieldbus or permanently set. Both are required for enabling the drive.-State. |
Motor brake closed unexpectedly. |
Check cabling and general functionality. |
Dynamic braking | |
|
Voltage exceeds motors rating. |
Drive bus voltage exceeds the motor’s defined voltage rating. |
Make sure that the motor fits the driving rating. |
Disable power stage | |
| n309 | Motor I2t load. reduce load | Motor I2t load (IL.MI2T) has exceeded the warning threshold IL.MI2TWTHRESH. This warning can only be generated in the case that the motor protection mode IL.MIMODE has been set to 1. | Reduce the load of the drive by adjusting lower acceleration / deceleration ramps. | None |
| F312 |
Brake released when it should be applied. |
Brake disengaged unexpectedly. | Check cabling and general functionality. | Controlled stop |
|
Failed to set feedback type. |
Feedback is not connected or wrong feedback type selected |
Check primary feedback (X10 connection). |
Dynamic braking | |
|
Analog signal amplitude fault. |
Analog signal amplitude is too low. Analog fault (resolver signal amplitude or sin/cos amplitude) |
Check primary feedback (X10 connection), resolver and sine/cos encoder only. |
Dynamic braking | |
|
EnDat communication fault. |
General communication problem with feedback. |
Check primary feedback (X10 connection), EnDat only. If feedback is linear, check calibration. |
Dynamic braking | |
|
Illegal Hall state (111, 000). |
Hall sensor returns invalid Hall state (111, 000); either all Hall sensors are on or off. Legal Hall states are 001, 011, 010, 110, 100, and 101. This fault can be caused by a broken connection in any one of the Hall signals. |
Check the feedback wiring; check all feedback connectors to ensure all pins are positioned correctly. |
Dynamic braking | |
| Bad communication with the feedback device.
|
Check primary feedback (X10 connection), Biss only. |
Dynamic braking | ||
|
BiSS multi cycle fault. |
||||
|
BiSS sensor fault. |
||||
|
SFDSmart Feedback Device configuration fault. |
Bad communication with the feedback device.
|
Internal feedback failure. Return to manufacturer for repair. |
Dynamic braking | |
|
SFD UART over run fault. |
Internal feedback failure. Return to manufacturer for repair. |
|||
|
SFD UART frame fault. |
Internal feedback failure. Return to manufacturer for repair. |
|||
|
SFD UART parity fault. |
Internal feedback failure. Return to manufacturer for repair. |
|||
|
SFD transfer timeout. |
Check primary feedback (X10 connection), SFD only. |
|||
|
SFD single corrupted position. |
Internal feedback failure. Return to manufacturer for repair. |
|||
|
General communication problem with feedback (internal feedback failure). |
Check primary feedback (X10 connection). Contact manufacturer for repair. |
Dynamic braking | ||
|
SFD transfer incomplete. |
General communication problem with feedback (internal feedback failure). |
Check primary feedback (X10 connection), SFD only. |
Dynamic braking | |
|
Broken wire in primary feedback. |
In primary feedback, a broken wire was detected (incremental encoder signal amplitude). |
Check feedback cable continuity. |
Dynamic braking | |
|
Primary feedback power supply. |
Power supply fault for primary feedback. |
Check primary feedback (X10 connection). |
Dynamic braking | |
|
Encoder init procedure failed. |
Phase find procedure did not complete successfully. |
Check encoder wiring, reduce/balance motor load prior to phase finding. |
Disable power stage | |
| F420 |
FB3 Endat communication fault. |
A communication error was detected with the EnDat 2.2 device connected to the X9 connector. | Check pinout and FB3 configuration and reconnect feedback. If problems persist, contact customer support. | Dynamic braking |
| F421 |
SFD resolver sensor fault. |
SensorA sensor is a type of transducer that converts one type of energy into another for various purposes including measurement or information transfer or sensor wiring failure inside motor. | Try resetting the fault. If it reappears return motor for repair. | Dynamic braking |
| F423 |
NV Failure – Extended Multiturn. |
The position saved in memory is corrupted. | Home axis or disable extended multiturn. If the fault persists, send the drive for repair. | Disable power stage |
|
n439 |
Deviation from predicted trajectory fault. |
Motor did not follow command values. Motor exceeded maximum allowed position following error (numeric). |
Check for increased load, jamming or sticking. Is position error set too low? |
Controlled stop |
|
n439 |
Following error magnitude fault. |
Motor did not follow command values. Motor exceeded maximum allowed position following error (user). |
Check feedback commutation setup and tuning parameters. |
Controlled stop |
|
Following error presentation. |
Motor did not follow command values. Motor exceeded maximum allowed position following error (presentation). |
Check feedback commutation setup and tuning parameters. |
Controlled stop | |
|
F451 n451 |
Feedback battery fault. |
The external battery voltage is too low. The F451 fault is generated if the AKD is not powered. The n451 warning is generated if the AKD is powered. This fault can be inhibited with FAULT451.ACTION. | Check or replace the external battery. | Dynamic braking |
| F452 | Extended Multiturn not supported with this feedback. | Non-multiturn feedback is connected while FB1.PMTSAVEEN is active. | Connect multiturn feedback to the drive or disable extended multiturn. | Disable power stage |
| F453 | Tamagawa communication fault (timeout). | Bad communication with the feedback device. Cabling or shielding fault, or internal feedback failure. | Check the cabling to the drive and if the problem persists then return the feedback to the manufacturer for repair. | Dynamic braking |
| F454 | Tamagawa communication fault (transfer incomplete). | |||
| F456 | Tamagawa communication fault (CRC). | |||
| F457 | Tamagawa communication fault (start timeout). | |||
| F458 | Tamagawa communication fault (UART Overrun). | |||
| F459 | Tamagawa communication fault (UART Framing). | |||
| F460 | Tamagawa encoder fault (over speed). | This fault is generated when the shaft is rotated above a maximum speed that can be maintained while the external battery is powered and the drive is powered off. | Reset the fault on the drive with DRV.CLRFAULTS. | Dynamic braking |
| F461 | Tamagawa encoder fault (counting Error). | When the feedback is powered on the position (within one revolution) was incorrect because of a problem with the feedback device. | Reset the fault on the drive with DRV.CLRFAULTS, if the problem persists then clean the feedback code plate. | Dynamic braking |
| F462 | Tamagawa encoder fault (counting overflow). | Multi-turn counter has overflowed. | Reset the fault on the drive with DRV.CLRFAULTS. | Dynamic braking |
| F463 | Feedback overheat fault. | The temperature of the encoder substrate exceeds overheating detection temperature during main power-on. | Reset the fault on the drive with DRV.CLRFAULTS after temperature of encoder is lowered. | Dynamic braking |
| F464 | Tamagawa encoder fault (multi-turn error). | Any bit-jump occurs in the multi-turn signal during main power-on. | Return to the origin. Reset the fault on the drive with DRV.CLRFAULTS. | Dynamic braking |
| F465 | Excessive shock detected by feedback device. |
1. Excessive shock from an impact or vibration has caused an error in the feddback device. or 2. Internal error in the feedback device mechanism, resulted in bad position data. |
1. Reduce external impacts to the motor housing and shaft. Tune the control loops filters. Reduce gains, particularly feed forward gains. Reduce maximum commanded acceleration. or 2. Replace the feedback device. |
Dynamic braking |
| F467 | Feedback fault on feedback 1 (See FB1.FAULTS for details). | The feedback device malfunctioned. |
Check FB1.FAULTS for detailed fault information. If using a BiSS feedback device, fault 467 indicates a communications fault with the BiSS feedback device. No additional information is available via FB1.FAULTS for this fault when using a BiSS feedback device. |
Dynamic braking |
| F469 | FB1.ENCRES is not power of two, Remote Commutation not possible. | Feedback Type 43 requires that the feedback resolution be a power of two. Feedback Type 43 is not supported for all feedback resolutions. | If the remote feedback device's resolution is a power of two, enter that value in FB1.ENCRES. Otherwise, choose a feedback device with a supported resolution (power of two) and enter that value in FB1.ENCRES. | Dynamic braking |
| F470 | Feedback fault on feedback 3. | Feedback is not connected or general communication problem. | Check tertiary feedback (X9 connection) | Dynamic braking |
| Field bus command velocity too high. | Fieldbus command velocity exceeds VL.LIMITP. | Lower fieldbus command trajectory, or increase the value of VL.LIMITP. | Disable power stage | |
| Field bus command velocity too low. | Fieldbus command velocity exceeds VL.LIMITN. | Increase fieldbus command trajectory, or decrease the value of VL.LIMITN. | Disable power stage | |
| F486 | Input change rate exceeds maximum speed of emulated encoder. | Motor velocity exceeds the maximum speed the emulated encoder output can generate. | Reduce value of DRV.EMUEPULSEWIDTH. | Controlled stop |
| F493 | Invalid commutation detected - motor accelerating in the wrong direction. Motor phase may be incorrect. | The velocity of the motor exceeded WS.CHECKV and the sign of the current was not equal to the sign of motor acceleration or the sign of motor velocity for a period of time larger than WS.CHECKT. |
1. Check motor phase wiring 2. Re-configure wake and shake (if Mode 0 or 1 is used) 3. Re-run wake and shake to determine correct commutation angle |
Dynamic braking |
|
n501 |
Bus over voltage. |
Bus voltage too high. Usually, this problem is load related. |
Reduce load or change motion profile. Check system regen capacity; add capacity if needed. Check mains voltage. |
Disable power stage |
|
Bus under voltage. Warning issued prior to fault. |
Bus voltage below threshold value. |
Check mains voltage. |
Controlled stop | |
|
n503 |
Bus capacitor overloaded. |
Single phase AC input on a drive only rated for three-phase input or excessive single-phase power load. |
Check mains voltage. |
Controlled stop |
|
1V2 over voltage. |
Internal supply voltage fault detected. |
Check wiring for electromagnetic compatibility (EMC). If issue persists exchange drive.
|
Controlled stop | |
|
1V2 under voltage. |
||||
|
2V5 over voltage. |
||||
|
2V5 under voltage. |
||||
|
3V3 over voltage. |
||||
|
3V3 under voltage. |
||||
|
5V0 over voltage. |
||||
|
5V0 under voltage. |
||||
|
+12V0 over voltage. |
||||
|
+12V0 under voltage. |
||||
|
-12V0 over voltage. |
||||
|
-12V0 under voltage. |
||||
|
Analog 3V3 over voltage. |
||||
|
Analog 3V3 under voltage. |
||||
|
Regen short circuit. |
Regen resistor short circuit. |
Regen IGBT short circuit. Contact technical support. |
Disable power stage | |
|
n521 |
Regen over power.
|
Too much power stored in regen resistor. |
Either get larger regen resistor or use DC bus sharing to dissipate power. |
Disable power stage |
|
Bus over voltage FPGA. |
Bus over voltage hard fault. |
Check mains voltage and check system brake capacity. |
Disable power stage | |
|
n524 |
Drive Foldback. |
Maximum drive power has been exceeded. The power has been limited to protect the drive. |
Motion requires too much power. Change profile to reduce load . |
Controlled stop |
|
Output over current. |
Current exceeds drive peak. |
Check for short or feedback faults. |
Disable power stage | |
|
Current sensor short circuit. |
1. Current sensor short circuit. 2. Motor cable plugged in upside down |
1. Restart drive. If issue persists, contact technical support. 2. Plug in cable right-side up. |
Disable power stage | |
|
Iu current AD converter stuck. |
Hardware failure detected. |
Restart drive. If issue persists, contact technical support. |
Disable power stage | |
|
Iv current AD converter stuck. |
Hardware failure detected. |
Restart drive. If issue persists, contact technical support. |
Disable power stage | |
|
Iu current offset limit exceeded. |
Hardware failure detected. |
Restart drive. If issue persists, contact technical support. |
Disable power stage | |
|
Iv current offset limit exceeded. |
Hardware failure detected. |
Restart drive. If issue persists, contact technical support. |
Disable power stage | |
|
Power stage fault. |
Hardware failure detected. |
Restart drive. If issue persists, replace drive. |
Disable power stage | |
|
Drive motor parameters setup incomplete. |
Before a motor can be enabled, you must configure a minimum set of parameters. These parameters have not been configured. |
Issue the command DRV.SETUPREQLIST to display the list of the parameters that you must configure. Configure these parameters either manually or automatically. You can manually configure these parameters in three ways: (1) set each parameter individually; (2) use the setup wizard to select the motor; or (3) select the motor type from the motor data base in the Motor window (MOTOR.AUTOSET must be set to 0 (off)). If you use the Motor window, you must first select the feedback type. If the motor has Biss Analog, Endat, or SFD feedback (feedback with memory), then these parameters are set automatically when MOTOR.AUTOSET is set to 1 (on). |
Disable power stage | |
|
Failed to read motor parameters from feedback device. |
Motor either does not have motor feedback memory, or the motor feedback memory is not programmed properly so the parameters cannot be read. |
Try to read parameters again by clicking the Disable and Clear Faults button, or by issuing the DRV.CLRFAULTS command. If this attempt is not successful, then set MOTOR.AUTOSET to 0 (off) and program the parameters using the setup wizard or manually set up the parameters. If the motor has motor memory (Biss Analog, Endat, and SFD motors have motor memory), return the motor to have the memory programmed. |
Dynamic braking | |
| F535 | Power-board over-temperature fault. | The power-board temperature sensor indicates more than 85 °C. | Reduce the load of the drive or ensure better cooling. | Disable power stage |
| F537 | Precharge fault. | Precharge process could not be performed in a reasonable amount of time. | Look for a shortcut in the string (cable) or exchange hardware | Disable Drives and Unpower Strings |
| F541 | AC input phase 1 missing. | Mains supply failure detected, phase L1 missed. | Check power connector and power source. | Disable Drives and Unpower Strings |
| F542 | AC input phase 2 missing. | Mains supply failure detected, phase L2 missed. | Check power connector and power source. | Disable Drives and Unpower Strings |
| F543 | AC input phase 3 missing. | Mains supply failure detected, phase L3 missed. | Check power connector and power source. | Disable Drives and Unpower Strings |
| F560 | Regen near capacity, could not prevent over voltage. | An F501 Bus Over Voltage has occured while the Regen Resistor was at or above 75% of its dissipation capacity. | Increase the size of regen resistor to be able to dissipate more power. | Disable power stage |
| F570 | Phase loss. | Phase loss detected. | Check mains power voltage. Fault action configurable by FAULT570.ACTION on pg. 1. | Disable power stage |
| n582 | Velocity has been limited commutation speed to less than 600Hz to meet ECCN 3A225 requirements. | Motor Velocity has exceeded the allowed commutation speed (599Hz). | Refer to ECCN 3A225 Limitations for Induction Motors. | Velocity command will be clamped at ECCN 3A225 regulation. |
| n601 | ModbusModBus is a serial communications protocol and is now the most commonly available means of connecting industrial electronic devices. ModBus is often used to connect a supervisory computer with a remote terminal unit in supervisory control and data acquisition (SCADA) systems. Versions of the ModBus protocol exist for serial port and Ethernet (it is widely used with TCP/IP over Ethernet) data rate is too high. | Modbus controller data rate is too high. | Reduce data rate. | Disable power stage |
|
Safe torque off. |
Safe torque off function has been triggered. |
Reapply supply voltage to STO if safe to do so. |
Disable power stage | |
| n603 | OPMODE incompatible with CMDSOURCE | This warning is generated when the drive is enabled and the gearing command source is selected at the same time as torque or velocity op-mode. | Select a different DRV.OPMODE andDRV.CMDSOURCE combination. | Disable power stage |
| n604 | EMUEMODE incompatible with DRV.HANDWHEELSRC. | Emulated encode mode is incompatible with the selected handwheel source. | Select a compatible emulated encode mode or change handwheel source. | Disable power stage |
| F621 | Control Board CRC fault. | Communications with the Power Board Failed | DRV.CLRFAULTS. If issue persists, contact technical support. | Disable power stage |
| F623 | Power Board CRC fault. | |||
| F624 | Power Board Watchdog fault. | |||
| F625 | Power Board Communication fault. | |||
| F626 | Power Board FPGA not configured. | |||
| F627 | Control Board Watchdog fault. | |||
|
FPGA cyclic read fault. |
FPGA-to-firmware data access error. |
DRV.CLRFAULTS. If issue persists, contact technical support. |
Disable Power Stage | |
|
Runtime communication fault. |
Check fieldbus connections (X11), settings, and control unit. |
Controlled stop | ||
|
n702 |
Fieldbus Communication lost.
|
All fieldbus communication was lost. |
Check fieldbus connections (X11), settings, and control unit. |
Controlled stop |
|
Emergency timeout occurred. |
Motor did not stop in the timeout defined. |
Change timeout value, change stop parameters, improve tuning. |
Disable power stage |
|
Copyright © 2015 Kollmorgen™ |
|